Offline Emulation
A device may be simulated by creating an Offline emulation of the device when starting a new project or by adding a device. This allows you to define and work with any of the available AKD2G devices, letting you perform device configuration without actually being connected. Select the options that match the device you will be configuring. The model number near the bottom of the dialog updates based on your selection. Lastly, choose a firmware version to emulate.
The configuration you have created offline can be pushed to an online device by connecting to it. If the devices match (based on the model number) you will be prompted to synch the parameters.
Additionally, changes made to an online device can be pushed to the offline version. See Parameter Synchronization for more information.